To run the ADP example follow the steps below.
Todo:
- Open Atmel Studio
- Select File → New → Example
Project
- Browse to, or search for the
ADP example application - SAM D21 Xplained Pro and select it
- Choose the preferred folder and
give the project a name, then click OK to create the
project
The project will be generated, then it is just a matter of compiling it and
programming it into the target board.
Todo:
- Open the project properties (right click the project in the
Solution Explorer and select
Properties)
- On the
Tool tab, select the appropriate tool and
interface
Todo:
- Click Start Without
Debugging (Debug → Start Without Debugging)
Todo: Open
the Data Visualizer as an extension inside Atmel Studio by selecting it in the
Tools menu.
Todo:
- In the DGI Control Panel, select
SAM D21 Xplained Pro
- Select the Autodetect
protocols box
- Click
Connect
You should see something like the screenshot below in the Data
Visualizer.