The Graph element has one sink endpoint for each plot. The endpoints accepts all numerical data types.
Each plot in the Graph can be shown or hidden dynamically by clicking the legend corresponding to the plot at the bottom of the Graph element. Hidden plots have a gray legend compared to visible plots having the same color on the legend as the plot itself.
In the graph above the plot SPI Output is visible while the plot TWI Output is hidden.