The data stream is processed in the same order as the configuration file specifies. All data must be given as little endian values, meaning that the lowest byte must be sent first. Additionally, a wrapper consisting of one byte before and one byte after the data stream variables must be added. This wrapper is used by the interpreter to synchronize to the data stream. The start byte can be of an arbitrary value except 0x5F, which is reserved for Auto-Configuration, but the end byte must be the inverse of the Start byte. For more information on the Auto-Configuration feature see Auto-Configuration and Auto-Configuration Example. The configuration file shall not define the start and end bytes.