To demonstrate how to use the Graph
module an example with a Night mode switch will be used. An ATmega256RFR2 Xplained Pro
with an I/O1 Xplained Pro extension is suitable as target hardware. The I/O1 extension
board features a light sensor that can be used to detect whether it is night or day.
This information can be used, for example, to switch a lamp on when the surroundings
turn dark.
The example requires the following equipment and software:
- Host computer with Atmel Studio 7 or
later installed (Data Visualizer is included)
- ATmega256RFR2 Xplained Pro kit
- I/O1 Xplained Pro extension
To run the example, the following hardware setup is
required:
- I/O1 Xplained Pro extension
connected to ATmega256RFR2 Xplained Pro EXT1 connector
- USB cable connected from host
computer to ATmega256RFR2 Xplained Pro
A picture of the setup is shown below.