The TWI interface source contains the raw values received on the TWI interface. The sink sends values received back out on the TWI interface. For further details on the physical part of the TWI interface, see the user guide of the debugging tool to be used to sample the TWI data.
The TWI Configuration dialog is opened from the TWI interface in the DGI Control Panel.
Field Name | Values | Usage |
---|---|---|
Address | 0-127 | TWI slave address |
Speed | 100000, 400000 | Speed setting for TWI slave. Used for timing. |
Enable timestamping | ON, OFF | Data is timestamped through the DGI timestamp interface (yields a slower transfer rate) |