The current consumption of the TA100 device can be measured by using the
AC164166
14-Pin SOIC socket board. The only devices on the board that will
consume power are the TA100 socketed device, the Power LED and the I
2C
pull-up resistors. Follow these steps to measure the current:
- 1.Modify the board to remove the
resistor, R1, which is in series with the LED. This will remove the current
through the LED from the total measured current.(1)
- 2.Install the TA100 device into the
socket.
- 3.Install the socket board into the
host system with the appropriate power settings.
- 4.Select either 3.3V or 5V power
for the measurement.(2)
- 5.Connect the high side of the
ammeter to the 3.3V or 5V supply.
- 6.Connect the low side of the
ammeter to the common PWR signal of the header.
- 7.Current measurements can now be
taken by running various TA100 commands and measuring the current.
(3)
Notes:
- 1.For lower accuracy current
measurements, this resistor may be kept in the circuit. It is recommended
that a separate measurement of the current through just the LED path be made
prior to measuring the TA100 device currents. This value can, then, be
subtracted from the total current measured.
- 2.The host board provides power
to the mikroBUS extension board, so whichever supply is selected must match
the capabilities and setting used on the host board.
- 3.When measuring the current of
I2C devices, the measurement will include the I2C
pull-up currents used to pull up the bus. For SPI signals, the pull-ups are
internal to the device and will also factor into the total current
consumed.