Creating the MPLAB X Project
- 1.Create a new stand-alone project (see
Create New Project) in MPLAB X using the ATmega4808 as the device (see
Selecting a Device); the PKOB nano as a programming tool (see Selecting a Programmer); and the XC8 or AVR GCC as a
compiler (see Selecting a Compiler). Finally, name the MPLAB project and
its location (see Naming a New Project). The Start page of MPLAB X will then
appear.
- 2.On the MPLAB X toolbar, look for and
click the MPLAB®\ Code Configurator (MCC) Icon
() or click Tools > Embedded > MPLAB X Code Configurator v3
Open/Close. For assistance with installation, refer to MPLAB ® Code Configurator Page (www.microchip.com/mplab/mplab-code-configurator)
- 3.Under Device Resources, scroll down
to the Internet of Things header. Under Examples, double click on
AVR-IoT Google Sensor Node(see MCC Start Page).
Figure 1. Create New Project
Figure 2. Selecting a Device
Figure 3. Selecting a Programmer
Figure 4. Selecting a Compiler
Figure 5. Naming a New Project
Figure 6. MCC Start Page