The AVR-IoT WG development board can be connected to a computer using a standard Micro-USB cable. Once plugged in, the LED array at the top right-hand corner of the board should flash twice in the following order: Blue, Green, Yellow, and Red. When the board is not connected to Wi-Fi , the blue LED will blink continuously. The board will appear as a Removable Storage Device on the host PC, as shown in Curiosity Board as Removable Storage. Double click the CURIOSITY drive to open it and get started.
Double click on the CLICK-ME.HTM file to enter the dedicated webpage to access the web application.