Memory Timing

The Memory Timing tab sets the timing parameters, which are then translated to the appropriate configuration values for the DDR subsystem IP, as shown in the following figure.

Figure 1. DDR Configurator—Memory Timing Tab