DDR3 Routing Topology

The following figure shows the FlyBy termination of the DDR3 address, command, and control signals (ACC).

Figure 1. DDR3 ACC Signals Fly By Termination

The following figure shows the FlyBy termination of the DDR3 clock signal.

Figure 2. DDR3 Clock Signal FlyBy Termination

The following figure shows the Point-to-Point routing of the DDR3 data signal.

Figure 3. DDR3 Data Signal Point-to-Point