To use the libraries, install the MPLAB             Code Configurator plug-in tool in the MPLAB X IDE.         This section describes the installation of MCC and the IEC60730 Class B Diagnostic         Libraries.
An update may be required if the library was installed previously and a new version         is available. This section describes how to update the library using CMT in MCC.
This section describes adding diagnostic tests using MCC Melody and the IEC60730         Class B Diagnostic Libraries in MPLAB X projects.
Examples are available for each diagnostic test. Users can generate these examples if         the options are enabled in the user interface. For instance, to add the PIC16/18 CPU         register diagnostic example: