The value of NVMREGS is set to ‘1
’ to access these regions. The memory
regions listed above would be pointed to by PC[15] = 1
, but not all
addresses reference valid data. Different access may exist for reads and writes. Refer
to the table below. When read access is initiated on an address outside the parameters
listed in the following table, the NVMDATH: NVMDATL register pair is cleared, reading back ‘0
’s.
Address | Function | Read Access | Write Access |
---|---|---|---|
0x8000 - 0x8003 | User IDs | Yes | Yes |
0x8005 - 0x8006 | Device ID/Revision ID | Yes | No |
0x8007 - 0x800B | Configuration Words 1-5 | Yes | Yes |
0x8100 - 0x82FF | DIA and DCI | Yes | No |
; This write routine assumes the following:
; 1. A full row of data are loaded, starting at the address in DATA_ADDR
; 2. Each word of data to be written is made up of two adjacent bytes in DATA_ADDR,
; stored in little endian format
; 3. A valid starting address (the LSb’s = 00000) is loaded in ADDRH:ADDRL
; 4. ADDRH and ADDRL are located in common RAM (locations 0x70 - 0x7F)
; 5. NVM interrupts are not taken into account
BANKSEL NVMADRH
MOVF ADDRH,W
MOVWF NVMADRH ; Load initial address
MOVF ADDRL,W
MOVWF NVMADRL
MOVLW LOW DATA_ADDR ; Load initial data address
MOVWF FSR0L
MOVLW HIGH DATA_ADDR
MOVWF FSR0H
BCF NVMCON1,NVMREGS ; Set PFM as write location
BSF NVMCON1,WREN ; Enable writes
BSF NVMCON1,LWLO ; Load only write latches
LOOP
MOVIW FSR0++
MOVWF NVMDATL ; Load first data byte
MOVIW FSR0++
MOVWF NVMDATH ; Load second data byte
CALL UNLOCK_SEQ ; If not, go load latch
INCF NVMADRL,F ; Increment address
MOVF NVMADRL,W
XORLW 0x1F ; Check if lower bits of address are 00000
ANDLW 0x1F ; and if on last of 32 addresses
BTFSC STATUS,Z ; Last of 32 words?
GOTO START_WRITE ; If so, go write latches into memory
GOTO LOOP
START_WRITE
BCF NVMCON1,LWLO ; Latch writes complete, now write memory
CALL UNLOCK_SEQ ; Perform required unlock sequence
BCF NVMCON1,LWLO ; Disable writes
UNLOCK_SEQ
MOVLW 0x55
BCF INTCON,GIE ; Disable interrupts
MOVWF NVMCON2 ; Begin unlock sequence
MOVLW 0xAA
MOVWF NVMCON2
BSF NVMCON1,WR
BSF INTCON,GIE ; Unlock sequence complete, re-enable interrupts
RETURN