3 Launching the Pre-Installed Webserver Application

To launch the pre-installed Webserver application, perform the following steps:
  1. Connect an Ethernet cable to J2 and connect it to the same router as your PC.
  2. Using Linux console as the command-line interface, change to the webserver directory.
    $ cd /opt/microchip/iiohttpserver
  3. Find the IP address of the icicle kit by running.
    $ ifconfig
  4. Launch the web server by running the script.
    $ ./run.sh
  5. The webserver will now start running.
  6. Browse to the IP address of the Icicle kit from your host machine to view the webpage.
Important: Click MPFS Icicle Kit User Guide to update your PolarFire SoC Icicle kit to the latest binaries.