5 Generating Two PWM Signals in Split Mode
A TCA instance can be split into two completely independent 8-bit timers. This feature provides a high degree of flexibility, being extremely helpful in waveform generation applications. Except for the cases where high accuracy signals are required, most of the applications can be designed using 8-bit signal generators, and the possibility of adding one more generator to the design can be a huge advantage. Though, there are more limitations in the Split mode than the Counter registers dimension. The most important one is that both 8-bit timers have only the down-count option, so the Dual-Slope PWM mode becomes unavailable. Also, the buffering scheme cannot be used, and the timers can no longer count events, only clock ticks. Moreover, there are no interrupts or flags for high-byte Compare registers. Regardless of these limitations, the Split mode can be attractive when there is a need for a high number of timers. The block diagram of the TCA in Split mode is provided below.
This mode will be put forward by generating two PWM signals with different frequencies and different duty cycles.
- The TCA corresponding register in
Port Multiplexer can be set to rout the module outputs to different ports. In this
case, Port A is chosen, which is also the default
port.
PORTMUX.TCAROUTEA = PORTMUX_TCA0_PORTA_gc;
Figure 5-2. TCAROUTEA Register - Enable the Split mode by setting the
corresponding bit in the CTRLD
register.
TCA0.SPLIT.CTRLD = TCA_SPLIT_SPLITM_bm;
Figure 5-3. CTRLD Register - The CTRLB register contains the
Enable bits of the compare channels. In this example, channel 0 of the lower byte of
the timer and channel 0 of the higher byte of the timer are
used.
TCA0.SPLIT.CTRLB = TCA_SPLIT_HCMP0EN_bm | TCA_SPLIT_LCMP0EN_bm;
Figure 5-4. CTRLB Register - Split Mode - In this mode, the Period register and
the Compare registers are split in half. Each half of the Period register determines
the frequency of the respective PWM signal. Using the desired frequency value, the
Period register value can be deduced from the following formula:
TCA0.SPLIT.LPER = 0xCF; TCA0.SPLIT.HPER = 0x44;
- Each half of the Compare registers
determines the duty cycle of the respective PWM
signal.
TCA0.SPLIT.LCMP0 = 0x68; TCA0.SPLIT.HCMP0 = 0x11;
- From the CTRLA register, the
prescaler is set to 16. To start the counter, the user must set the Enable bit in
the same
register.
TCA0.SPLIT.CTRLA = TCA_SPLIT_CLKSEL_DIV16_gc | TCA_SPLIT_ENABLE_bm;
- The initialization code provided
illustrates a simple way of configuring the TCA in Split mode, but some mentions
must be made. The Single Slope PWM mode is the only Waveform Generation mode
available. Also, it is recommended to stop the timer and to do a hard Reset before
switching from Normal mode to Split mode. An example is provided below. Clear the
Enable bit in the CTRLA register to stop the counter. Then, in the Command bit field
of the CTRLESET register, the user will write the code of the hard Reset
command.
void TCA0_hardReset(void) { TCA0.SINGLE.CTRLA &= ~(TCA_SINGLE_ENABLE_bm); TCA0.SINGLE.CTRLESET = TCA_SINGLE_CMD_RESET_gc; }
- Then, pins 0 and 3 of Port A (PA0 and
PA3) are set as outputs by writing a ‘
1
’ to each corresponding bit in the Direction register of the port.PORTA.DIR |= PIN0_bm | PIN3_bm;
An MCC generated code example for AVR128DA48 with the same functionality as the one described in this section can be found here: