1.4.1 Bootloader and Application Binary Merge Script Help

This document describes the usage of btl_app_merge_bin.py host script.

Downloading the Host Script

To clone or download the host tools from Github, go to the bootloader repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions.

Path of the tool in bootloader repository is tools/btl_app_merge_bin.py.

Setting Up the Host PC

The script is compatible with Python 3.x and higher.

Description

  • This script should be used to merge the bootloader binary and application binary
  • It creates a merged binary output where bootloader is placed from start and the application will be placed at the offset passed as parameter
  • If the application offset is not equal to end of bootloader offset it fills the gap with 0xFF until the application offset
  • The merged binary can be used by CAN NVM Host Application as input for Updating bootloader and application together
  • The merged binary will be created in the directory from where the script was called

Usage Examples

Below is the syntax to show help menu for the script:

python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py --help
Below is the syntax and an example on how to merge a bootloader binary and application binary:
python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py -o <Offset> -b <Bootloader_binary_path> -a <Application_binary_path>
python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py -o 0x2000 -b <harmony3_path>/bootloader_apps_can/apps/can_fail_safe_bootloader/bootloader/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin -a <harmony3_path>/bootloader_apps_can/apps/can_fail_safe_bootloader/test_app/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin