2 Results
In this white paper, the benchmarking results are derived by executing both CELT and SILK mode, that is, Hybrid mode simultaneously on the PolarFire SoC Icicle kit. The following table lists the benchmarking results.
| Benchmarking | Result | |
|---|---|---|
| CELT and SILK (Hybrid mode) | Code Space | 194.142 Kbytes |
| Data Space | 53.37 bytes (BSS + Sdata + Read only data) | |
| Throughput | 99% |
| Section | Size |
|---|---|
| Text | 194142 |
| Read Only Data (rodata) | 52048 |
| Segment Data (sdata) | 1310 |
| Block Started by Symbol (BSS) | 16 |
The Opus codec test suite has 14 test cases, such as CELT, SILK, Opus_api, Opus_decode, Opus_encode, padding, project test cases ref RFC 6716, and so on. All these standard test cases are executed on the PolarFire SoC Icicle kit with the throughput of 99%.
The following figure shows the Opus codec test suite summary for PolarFire SoC Icicle Kit.

The following figure shows the log for Mono-Opus Audio Codec.
The following figure shows the log for Stereo-Opus Audio Codec.