1.22 RNG Random Number
This example application shows how to use the RNG Peripheral library to generate a pseudo-random number.
Description
The RNG peripheral has two blocks. One of them is called True Random Number Generator (TRNG) and the other is called Pseudo-Random Number Generator (PRNG). The TRNG generates true random numbers that can be used as seed for the PRNG. The PRNG can generate random numbers of up to 64-bits of length. This application shows how to generate a 64-bit pseudo-random number with the help of PRNG and TRNG.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/rng/rng_random_number/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mz_ef_sk.X | MPLABX project for PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mz_ef_sk.X | PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit |
Setting Up PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit
- Connect mini USB cables from the ‘Debug USB’ and ‘USB-to-UART’ connectors on the board to the computer
Running the Application
- Open the Terminal application (Ex.: Tera term) on the computer
- Connect to the EDBG Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE
- Press the switch to generate a 64-bit pseudo-random number (Refer to the table
below for switch details)
Board Switch Name PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit SW1 - Observe the following output in the console: