1 Harmony 3 Driver and System Service Application Examples for SAM9X7 Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.
| Name | Description |
|---|---|
| Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
| FAT Filesystem throughput using SDMMC Media | This application calculates throughput by Writing and Reading data into a SD-Card at High Speed using the MPLAB Harmony File System and the SDMMC driver |
| FAT Filesystem using RAM Media | This application shows an example of using the MPLAB Harmony File System to access RAM media |
| FAT Filesystem using SDMMC Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDMMC driver |
| FAT Filesystem using SST26 Media | This application shows an example of using the FAT File System to access SQI based SST26 flash media |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| FreeRTOS Task Notification | This example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore |
| I2C Driver Synchronous - I2C EEPROM | This example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM |
| I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
| SDMMC Driver Asynchronous - SDIO Read Write | This example application shows how to use the SDMMC driver in asynchronous mode to perform read/write operations using SDIO interface on the SD Card Media |
| SDMMC Driver Asynchronous - SDMMC Read Write | This example application shows how to use the SDMMC driver in asynchronous mode to perform block operations on the SD Card Media |
| SMC NAND Flash Driver - NAND Flash Read Write | This example application shows how to use the NAND Flash driver to perform read and write operations on NAND Flash device. |
| SPI EEPROM AT25 Driver - EEPROM Read Write | This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |