2.4.3.3 BL_CopyImageAreas()
bl_result_t BL_CopyImageAreas (uint8_t srcImageId, uint8_t destImageId)
Performs a direct internal memory copy of one image space to another.
| in | srcImageId |
- Image ID that identifies the source image space |
| in | destImageId |
- Image ID that identifies where the source image space will be copied to |
BL_PASS - Image copy operation finished successfully BL_FAIL - Image copy operation failed unexpectedly BL_ERROR_INVALID_ARGUMENTS - Invalid image ID was used as an argument BL_ERROR_COMMAND_PROCESSING - Copy operation failed at the memory layer |