2.6.3.3 BL_FlashCopy()
bl_mem_result_t BL_FlashCopy (flash_address_t srcAddress, flash_address_t destAddress, size_t length)
Helper function to enable the direct copying of one Flash area to another.
| in | srcAddress |
- Starting address of the source data for the Flash copy operation |
| in | destAddress |
- Starting address of the destination for the Flash copy operation |
| in | length |
- Total number of bytes to be copied to the destination address |
BL_MEM_PASS - Flash write succeeded BL_MEM_FAIL - Flash write failed BL_MEM_INVALID_ARG - An invalid argument is passed to the function |