2.2.3.1 COM_FrameSet()
com_adapter_result_t COM_FrameSet (uint8_t * responseBufferPtr, uint16_t responseLength)
Transfers bytes from the given buffer using the defined framing format.
| in | responseBufferPtr |
- Pointer to the buffer that needs to be sent |
| in | responseLength |
- Length of the response that needs to be sent |