2.3.14 PHY_StartContinuousTransmit Function
C
void PHY_StartContinuousTransmit(PHY_ContinuousTxMode_t txMode,
bool randomContent)
Summary
Starts continuous transmission on current channel
Description
This function is called to start the continuous transmission on current channel.
Precondition
PHY_Init() should have been called before calling this function.
Parameters
Param | Description |
---|---|
txMode | Mode of continuous transmission |
CW_MODE - Continuous Wave mode to transmit the signal at Fc +&- 0.5MHz frequency | |
PRBS_MODE - PRBS mode to Pseudorandom Binary Sequence frame continuously | |
randomContent | Use random content if true |
Returns
None
Example
PHY_Retval_t retVal = PHY_FAILURE; uint8_t phyChannel = 15; PHY_ContinuousTxMode_t txMode = CW_MODE; bool useRandomContent = false; PibValue_t pibValue; // Setting Current channel pibValue.pib_value_8bit = phyChannel; retVal = PHY_PibSet(phyCurrentChannel, &pibValue); if(PHY_SUCCESS == retVal) { //Start continuous tx in CW mode PHY_StartContinuousTransmit(txMode, useRandomContent); }
Remarks
None