2.3.21 PHY_ConfigRxRPCMode Function

C

PHY_Retval_t PHY_ConfigRxRPCMode(uint8_t rxRPCEnable)

Summary

Configures the reduced power consumption mode

Description

The function is used to configure the reduced power consumption mode of the receiver

Precondition

PHY_Init() should have been called before calling this function.

Parameters

ParamDescription
rxRPCEnable0x01 - To Enable the rxRPC mode
0x00 - To disable the rx RPC mode

Returns

PHY_SUCCESS If trx is configured correctly PHY_FAILURE otherwise

Example

PHY_Retval_t retVal = PHY_FAILURE;
uint8_t rxRPCEnable = 0x01;

retVal = PHY_ConfigRxRPCMode(rxRPCEnable);
if(PHY_SUCCESS == retVal)
{
    //Trx is configured to reduced power consumption mode
}

Remarks

None