1.4 FAT Filesystem using SD Card Media

This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB.

Description

File System Operations on the SD Card:

  • Application opens a file named FILE_TOO_LONG_NAME_EXAMPLE_123.JPG in the root directory of the SD card and reads its content into memory
    • The image file could be any arbitrary JPEG (image) file chosen by the user and then renamed to FILE_TOO_LONG_NAME_EXAMPLE_123.JPG
  • Application creates directory named Dir1 in the root directory
  • Application creates a new file named FILE_TOO_LONG_NAME_EXAMPLE_123.JPG inside Dir1
  • Application copies the content from step 1 into this newly created file
The reason for choosing a JPEG file for test purposes is that the duplicate file, Dir1/FILE_TOO_LONG_NAME_EXAMPLE_123.JPG created by the demonstration could be easily verified for correctness.If the new file inside Dir1 opens for viewing on the computer and matches to original image, the test is deemed to have passed. Otherwise, if the file does not open (i.e., is corrupted), the test will be considered to have failed.
Note: Since the application creates a directory named Dir1, it is important that the a folder with the same name does not exist on the SD card. If a directory named Dir1 is already present on the SD card, the application will fail.

File system layer uses:

  • SDSPI Driver to communicate to SD Card over SPI interface.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/fs/sdspi_fat/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_l21_xpro_freertos.XMPLABX project for SAM L21 Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_l21_xpro_freertos.X SAM L21 Xplained Pro Evaluation Kit

Running the Application

  1. Build and program the application using its IDE
  2. Press Switch to start the file operations
  3. The LED is turned ON if there was no error during creating the directory and copying the file into it
Refer to the following table for Switch and LED names:
BoardSwitch NameLED Name
SAM L21 Xplained Pro Evaluation KitSW0LED0