1.8 SPI Driver Asynchronous - Multi Instance
This example application demonstrates the multi instance feature of the asynchronous mode of the SPI driver by reading and writing to two EEPROMs connected to two different SPI bus.
Description
This application uses the asynchronous mode of the SPI driver and demonstrates the multi instance feature by reading and writing to two EEPROMs connected to two different SPI bus.
The application communicates with two EEPROM 3 click boards that has AT24CM02 EEPROM on it.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/spi/async/spi_multi_instance/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_l21_xpro.X | MPLABX project for SAM L21 Xplained Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_l21_xpro.X | SAM L21 Xplained Pro Evaluation Kit |
Setting Up SAM L21 Xplained Pro Evaluation Kit
- To run the demo, the following additional hardware are required:
- Install EEPROM 4 click boards on the mikroBUS Xplained Pro boards
- Connect the mikroBUS Xplained Pro boards on EXT1 and EXT2 headers of the SAM L21 Xplained Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and Program the application using its IDE.
- The LED indicates success or failure.
- The LED turns ON when the data read from the EEPROMs matches with the data written to the EEPROMs.
| Board | LED Name |
|---|---|
| SAM L21 Xplained Pro Evaluation Kit | LED0 |