Added a compiler limitation note
for the exp2(), exp2l(), and
exp2f() functions, since they have been removed from the
library shipped with the MPLAB XC8 compiler.
Added missing inclusion of
<stdio.h> in some examples performing file and
formatted IO operations.
Added missing inclusion of
<time.h> in examples using
localtime().
Clarified that time zones are not
supported by localtime().
Specified that <fenv.h> functionality is only available for
devices with a floating-point unit.
Indicated that the raise() function is only implemented as a
stub with MPLAB XC32 and clarified the usage of this function's example
code.
Clarified note regarding smart IO customization of formatted IO functions.
Corrected the prototype shown for the vsnprintf()
function.
Replaced description of the system() function.
Expanded the description of the
time() function.
Corrected the description for
getwc(), putwc(),
ungetwc() functions.
Corrected wide string array type
used in the example code for all functions implemented by
<wctype.h>.
Replaced example code for the vswscanf() function.
Clarified the general description in the Syscall Interface section.
Updated the applicability note used by some syscall interface functions that
they are additionally implemented by MPLAB XC16.
Added new section which indicates which functions are not thread safe.
Revision C (October 2023)
Added references to the MPLAB
XC-DSC compiler.
Corrected conversion specifiers
used with example code associated with ceill,
expl(), logbf(), and
logbl() functions.
Corrected example code for the
remquo() family of functions.
Updated information relating to
how the sqrt() family of functions is implemented for Cortex-M
devices.
Improved the description of the
offsetof() macro.
Removed undefined behavior
examples for ldiv() and lldiv()
functions.
Clarified the return value and
setting of errno for the strtod() family of
functions.
Added types for
clock_t and time_t, the latter which has
changed in recent XC8 compiler releases.
Revision D (September
2024)
Added the MPLAB XC32 form of the
option used to specify the heap size in brk() and
sbrk() descriptions
Indicated that the
brk() and sbrk() functions are deprecated
when using MPLAB XC32
Updated values in <limit.h> to accommodate new dsPIC33A
devices