1 Harmony 3 Driver and System Service Application Examples for PIC32CM LE/LS Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
| Name | Description |
|---|---|
| Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
| FAT File System using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT File System using SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
| SPI Driver Asynchronous - Multi instance | This example demonstrates how to use multi instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| TrustZone FreeRTOS Basic | This example application blinks an LED to show the FreeRTOS threads that are running in non-secure mode and to indicate status |
| USART Driver Asynchronous - UART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
| USART Driver Synchronous - UART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |