7 Appendix
Schematic, Assembly Drawing, Adapter Pinout, Programming External MCUs, External Debuggers
7.1 Schematic
7.2 Assembly Drawing
7.3 Curiosity Nano Base for Click boards™
7.4 Programming External Microcontrollers
Use the on-board debugger on AVR32SD32 Curiosity Nano to program and debug microcontrollers on external hardware.
7.4.1 Supported Devices
All external AVR® microcontrollers with the UPDI interface can be programmed and debugged with the on-board debugger with Microchip MPLAB X IDE.
External SAM, PIC16 and PIC18 microcontrollers having a Curiosity Nano Board can be programmed and debugged with the on-board debugger with Microchip MPLAB X IDE.
AVR32SD32 Curiosity Nano can program and debug external AVR32SD32 microcontrollers with MPLAB X IDE.
7.4.2 Software Configuration
No software configuration is required to program and debug the same device mounted on the board.
To program and debug a different microcontroller than the one mounted on the board, configure Microchip MPLAB X IDE to allow an independent selection of devices and programming interfaces.
- Navigate to through the menu system at the application top.
- Select the category in the options window.
- Check the Exclude device checks for kits option.

7.4.3 Connecting to External Microcontrollers
The figure and table below show where to connect the programming and debugging signals to program and debug external microcontrollers. The on-board debugger can supply power to the external hardware or use an external voltage reference for its level shifters. Read more about the power supply in Figure 4-11 4-13.
The on-board debugger and level shifters actively drive data and clock signals used for programming and debugging (DBG0, DBG1, and DBG2). Pull-down resistors are required on the ICSP™ data and clock signals to debug PIC® microcontrollers. All other interfaces are functional with or without pull-up or pull-down resistors.
DBG3 is an open-drain connection and requires a pull-up resistor to function.
- Connect GND and VTG to the external microcontroller
- Tie the VOFF pin to GND if the external hardware has a power supply
- Make sure there are pull-down resistors on the ICSP data and clock signals (DBG0 and DBG1) to support the debugging of PIC microcontrollers
Curiosity Nano Pin | UPDI | ICSP™ | SWD |
---|---|---|---|
DBG0 | UPDI | DATA | SWDIO |
DBG1 | — | CLK | SWCLK |
DBG2 | — | — | — |
DBG3 | — | MCLR | RESET |
7.5 Connecting External Debuggers
Even though there is an on-board debugger, external debuggers can be connected directly to the AVR32SD32 Curiosity Nano to program/debug the AVR32SD32. When not actively used, the on-board debugger keeps all the pins connected to the AVR32SD32 and board edge in tri-state. Therefore, the on-board debugger will not interfere with any external debug tools.
7.6 Disconnecting the On-Board Debugger
The on-board debugger and level shifters can be disconnected from the AVR32SD32.
The power supply block diagram (Figure 11) shows all connections between the debugger and the AVR32SD32. The signal names are printed in silkscreen on the top or bottom side of the board.
Cut the GPIO straps in Figure 4-12 to disconnect the debugger.
7.7 Getting Started with IAR™
IAR Embedded Workbench® for AVR® is a proprietary high-efficiency compiler not based on GCC. Programming and debugging of AVR32SD32 Curiosity Nano is supported in IAR™ Embedded Workbench for AVR using the Atmel-ICE interface. To get the programming and debugging to work, some initial settings must be set up in the project.
The following steps will explain how to get the project ready for programming and debugging:
- Make sure that the project to be configured is opened. Open the OPTIONS dialog for the project.
- In the category General Options, select the Target tab. Select the device for the project, or if not listed, the core of the device, as shown in Figure 7-10.
- In the category Debugger, select the Setup tab. Select Atmel-ICE as the driver, as shown in Figure 7-11.
- In the category Atmel-ICE 1 tab. Select UPDI as the interface. Optionally select the UPDI frequency, as shown in Figure 7-12. , select the