6.4 Info Command

The Info command accesses some static or dynamic status information from the device, depending on the parameters input to the command.The specific modes of information include:
Revision
Returns a value indicating the device identification byte and the revision number of the device. It is recommended that software not depend on the revision information as it may change over time.
KeyValid
Returns a value indicating the validity of an ECC private key . An ECC private key status can either be valid or invalid.
LockStatus
Returns a value indicating if the slot selected in either the Configuration or Data zone is locked or unlocked. After the Delete command has been run this mode will always fail.
ChipStatus
Returns a value. The first byte returned indicates if the Delete command has been used to clear the data slots.