3.1.4.1 diag_cpu_execution_mode_t
enum diag_cpu_execution_mode_t
Operating mode in which the DIAG_CPU_SelfTest diagnostic API function will be executed.
DIAG_CPU_SELF_TEST_SUBSET_1 |
Executes Subset 1 function within the current execution of the DIAG_CPU_SelfTest diagnostic API function |
DIAG_CPU_SELF_TEST_SUBSET_2 |
Executes Subset 2 function within the current execution of the DIAG_CPU_SelfTest diagnostic API function |
DIAG_CPU_SELF_TEST_SUBSET_3 |
Executes Subset 3 function within the current execution of the DIAG_CPU_SelfTest diagnostic API function |
DIAG_CPU_SELF_TEST_ALL |
Executes all test subsets sequentially within the current execution of the DIAG_CPU_SelfTest diagnostic API function. In this mode, only one invocation of the DIAG_CPU_SelfTest function is sufficient to fully perform the diagnostic function. |