1 MPLAB® Harmony Class B Library for PIC32CM JH Devices
The Class B Library provides APIs to perform self-tests for the on-board systems of the microcontroller.
Features Tested by the Class B Library
| Component |
Reference (Table H1 of IEC 60730-1) | Fault/Error | Acceptable Measures |
|---|---|---|---|
| CPU Registers | 1.1 | Stuck-at | Static memory test |
| CPU Program Counter | 1.3 | Stuck-at | Static memory test |
| Interrupts | 2 | No interrupt / too frequent interrupt | Functional test |
| CPU Clock | 3 | Wrong frequency | Frequency monitoring |
| Flash | 4.1 | All single bit faults | Modified checksum |
| SRAM | 4.2 | DC fault | Static memory test |
| SRAM data path | 5.1 | Stuck-at | Static memory test |
| SRAM data path | 5.2 | Wrong address | Static memory test |
| Digital I/O | 7.1 | Abnormal operation | Input comparison or output verification |
Class B Peripheral Library Usage
This topic describes the basic architecture of the Class B library and provides information and examples on how to use it. APIs defined by the Class B library can be used either by the start-up code or by the application code. The application may use PLIBs, drivers or middleware from the Harmony 3 software framework along with the Class B library code.
Abstraction Model
The following picture shows positioning of Class B library in a Harmony 3 based application.

Start-up vs. Run-time
The Class B library contains many self-test routines those can be executed at startup
and run-time. If a self-test is executed at startup, it is called as a Start-up
Self-test (SST) and if it is executed at run-time, then it is called a Run-time
Self-test (RST). There are a few self-tests which can be used only as SST or as RST,
such self-tests have SST or RST in the API name eg:
CLASSB_RST_IOTest(),
CLASSB_SST_InterruptTest(). If a self-test API does not have
SST or RST in its name, then it can be used at startup as well as runtime.
Start-up Self-test (SST)
SSTs are used to test a component inside the microcontroller before it is initialized
and used. When the Class B library is added via MPLAB® Code Configurator (MCC), the
selected SSTs are inserted into the _on_reset() function which is
called from the Reset_Handler(). This means that none of the data
initialization could have happened before running SSTs. So, the Class B library
initializes necessary variables before using them. It is not mandatory to test all
the components during startup. The SRAM can be tested partially if a faster startup
is needed by the application. In this case, modify the corresponding configuration
macro (CLASSB_SRAM_STARTUP_TEST_SIZE) present in
classb.h file to change the size of the tested area.
Run-time Self-test (RST)
RSTs can be used by the application during run-time to check safe operation of different components in the microcontroller. These tests are non-destructive. In the case of run-time tests, the application shall decide which test to execute when.
Components in the Library
The Class B library contains self-test routines for different components listed in Table 1-1.
Critical and Non-critical Components
Based on the impact of failure, different components inside this Class B library are categorized as critical or non-critical.
If the self-test for CPU registers, PC or Flash detects a failure, the code execution is
stopped, and it remains in an infinite loop. This is to prevent unsafe code execution.
In the case of non-critical components, a failsafe function
(CLASSB_SelfTest_FailSafe) is called when a failure is detected.
This function contains a software break point and an infinite loop. Further code shall
be added into this function as per the application need. The failsafe function must not
return to the Class B library, since it is called due to a self-test failure. Avoid use
of features which depend on the failed component. For example, if self-test for clock is
failed, it is not advisable to use UART for error reporting as BAUD rate may not be
accurate. In the case of SRAM failure, avoid the use of function calls or use of
variables in SRAM. A simple error reporting mechanism in this case of SRAM failure can
be toggling of an IO pin.
Critical Components
- CPU registers including the Program Counter
- Internal Flash program memory

Non-critical Components
- CPU clock
- IO pins
- Internal SRAM
- Interrupts

Self-tests for Components in the Library
CPU Registers
The ARM® Cortex®-M0+ is the CPU on the PIC32CM JH devices. The Class B library checks the processor core registers for stuck-at faults. The stuck-at condition causes register bit to remain at logic 0 or logic 1. Code execution should be stopped if this error condition is detected in any of the CPU registers.
This self-test follows the register save/restore convention specified by AAPCS. It can be used at startup as well as run-time. The Program Counter (PC) self-test is designed as a separate test since this register cannot be checked with usual test data patterns.

Program Counter (PC)
The self-test for PC checks whether a stuck-at condition is present in the PC register. The stuck-at condition causes register bit to remain at logic 0 or logic 1. Code execution should be stopped if this error condition is detected.
The self-test for PC calls multiple functions in predefined order and verifies that each function is executed and returns the expected value. If the return values of all test functions are correct, the Program Counter is assumed to be working fine. This self-test can be used at startup as well as run-time.

Flash
The internal flash memory of the device needs to be checked for proper functionality. The NVMCTRL embeds a functional safety feature in the form of a ‘single-error correction’ and ‘double-error detection’ (SECDED) Hamming Error Correction Code (ECC). This feature applies to the main Flash memory panel, the Data Flash, the User Row, the Software Calibration Area, and the Serial Number. Each single bit error in any 64-bit word of these sections will be corrected seamlessly by the NVMCTRL (and not written back in memory). Each double bit error will be detected but not corrected. For each 64-bit word in the memory, 8 bits are added in memory for storing the ECC. The standalone ECC logic comes with a fault injection and capture logic, used for testing the ECC feature.
The routine to enable the ECC feature on the Flash memory is available in the Class B library and this routine is called in the startup if it is selected via the Harmony 3 MCC configuration.
SRAM
The SRAM on the device is tested during runtime with the help ECC feature on the device. The ECC feature is enabled by default after a reset, and can then be disabled and re-enabled using the CTRLA.ENABLE bit. This disabling/enabling only applies to ECC decoding upon reads. The ECC encoding upon writes is always enabled and cannot be disabled. More details are available in the datasheet chapter MCRAMC. During the startup, the SRAM is tested by the Class B library with the help of the SMBIST peripheral.
Clock
The self-test for CPU clock checks whether the CPU clock frequency is within the permissible range. It uses RTC and SysTick to measure the CPU clock frequency. The RTC is clocked at 32768 Hz from the 32 kHz External Crystal Oscillator and CPU clock can be from any other high frequency oscillator. If the CPU clock frequency is within specified error limit, it returns PASS. The test duration is defined by one of the input arguments. The clock self-test can be used at startup as well as run-time.
- This self-test uses the RTC peripheral. Thus, if it is used during run-time, the RTC shall not be used by the application for continuous modes such as real time clock or calendar. If the RTC is used for some other purpose, it must be reconfigured after running the clock self-test.
- Keep the clock test duration lesser than the WDT timeout period, to avoid the WDT resetting the device.

Interrupt
The self-test for this element checks the interrupts functionality of the microcontroller. It configures the Nested Vectored Interrupt Controller (NVIC), the Real-Time Counter (RTC) and the Timer Counter 0 (TC0) peripherals to test the interrupt handling mechanism. It verifies that at least one interrupt is generated and handled properly. This self-test also checks whether the number of interrupts generated are too many within a given time period. It reports a PASS if the RTC has generated at least one interrupt and the total number of interrupts generated by the TC0 is greater than one and less than the specified upper limit. The clock used for RTC is 1kHz from the internal OSCULP32K and for TC0 the clock is same as the default CPU clock (48MHz from the DFLL48M). The interrupt self-test can be used only at startup.
- This startup self-test utilizes the interrupts generated by RTC and TC0. For run-time testing of interrupts, a separate self-test need to be developed.

IO pin
The self-test for IO pins verifies that any output pin is able to keep the configured logic state on the pin and any input pin is able to read the logic state present on the pin.
As the exact use of an IO pin is decide by the application, it is the responsibility of the application to configure the IO pin direction and drive the pin to the expected state before calling this self-test. Before testing an output pin, call CLASSB_IO_InputSamplingEnable() function to enable input sampling for the IO pin. When testing an input pin, ensure that the IO pin is externally kept at a defined logic state. The IO pin self-test can be used only at run-time.

Class B Peripheral Library - Timing of self-tests
| Name | Time (in microseconds) |
|---|---|
| CLASSB_CPU_RegistersTest | 20 |
| CLASSB_CPU_PCTest | 12 |
| CLASSB_RST_IOTest | 8 |
| CLASSB_ClockTest | 7650 |
| CLASSB_SST_InterruptTest | 13800 |
| Name | Time (in microseconds) | Tested size |
|---|---|---|
| SRAM Memory Built-In Self-Test (SMBIST ) | 3000 | 32 KB |
- Timing is measured using onchip peripherals (SysTick and TC) at optimization level -O1 with CPU running at 48MHz from the internal 48MHz oscillator. Before using these self-tests in an application it is recommended to check self-test timings with the required configuration (CPU clock, compiler optimization, memory size).
- During run-time, the internal Flash and the SRAM are monitored by the corresponding ECC peripherals. Thus no timing measurement is required.
- Following IDE and toolchain are used for timing measurements
- MPLAB X v6.10
- XC32 Compiler v4.30
Configuring the Library (MPLAB X)
This section provides details necessary to integrate the Class B library with other software components.
Optimization Requirements
The self-test routines provides by the Class B software does not have any specific optimization requirements.
Reserved SRAM area for the Class B library
Dedicated SRAM area is needed for the self-tests in the Class B library. This should help to prevent unintentional access to the area by the application. Initial 64 bytes of the SRAM 0x20000000 shall be reserved.
This reserved SRAM must not be accessed from outside the Class B library. To check or update test results, use the corresponding interface APIs. When the Class B library is added into the project with the help of MCC, the linker setting is modified by MCC as shown below. The numbers used in this example is for a device with 64kB of SRAM.
-DRAM_ORIGIN=0x20000040 -DRAM_LENGTH=0xffc0

Modified Startup Sequence
When generating project with help of MPLAB Harmony 3, the startup code is present in a
file named startup_xc32. This file contains the
Reset_Handler which has all startup code that runs before the
main() function. Initialization of the Class B library is done from
the _on_reset function which is the first function to be executed from
the Reset_Handler. The function named
CLASSB_Startup_Tests executes all startup self-tests inserted into
classb.c file by the MCC. If none of the self-tests are failed,
this function returns CLASSB_STARTUP_TEST_PASSED. If any of the startup
self-tests are failed, this function does not return because of the following reason. In
the case of critical failures (CPU registers or internal flash), the corresponding
self-test remains in an infinite loop to avoid unsafe execution of code. The self-tests
for SRAM, Clock and Interrupt are considered non-critical since it may be possible to
execute a fail-safe function after detecting a failure. In such case, the
CLASSB_SelfTest_FailSafe() function is called when a failure is
detected. Since the default implementation of CLASSB_SelfTest_FailSafe
routine contains an infinite loop, it won't return to the caller.
- The library defines the
_on_resetfunction and handles some of the reset causes. The application developer shall insert functions to handle the rest of the reset causes.
WDT Test and Timeout
The Watchdog timer is used as a recovery mechanism in case of software failures. The
Class B library enables the WDT and checks whether a WDT reset is issued if the timer is
not cleared. In CLASSB_Startup_Tests (in file
classb.c), before performing startup self-tests, the WDT timeout period
is configured. It can be modified after generating the project. During startup, the
device runs from 4 MHz internal clock. Before running any self-test which takes longer
time (SRAM or Flash test), configuring the CPU clock at 48 MHz will help to reduce the
execution time. If any of these self-tests takes more time than the WDT timeout period,
it results in a WDT reset. Thus, properly configuring the WDT period is essential during
startup as well as runtime.
Configuring Startup Tests via MCC
Clone the classb_pic32cm_jh repo. When an MPLAB Harmony 3 project is
created, the MCC lists all available components that can be added to the project. The
self-tests which need to run during startup can be configured via MCC. The
Configuration Options menu appears with a mouse click on the
Class B Library component inside the Project
Graph. The configurations done via MCC does not configure the library, instead
it helps to modify the input arguments and to decide whether to run a specific test
during startup.
Class B Library Interface
| Name | Description |
|---|---|
| CLASSB_CLOCK_DEFAULT_CLOCK_FREQ | Default CPU clock speed. |
| CLASSB_CLOCK_ERROR_PERCENT | Clock error percentage selected for startup test. |
| CLASSB_CLOCK_MAX_CLOCK_FREQ | Maximum CPU clock speed. |
| CLASSB_CLOCK_MAX_SYSTICK_VAL | Upper limit of SysTick counter. |
| CLASSB_CLOCK_MAX_TEST_ACCURACY | Maximum detectable accuracy for clock self-test. |
| CLASSB_CLOCK_MUL_FACTOR | Multiplication factor used in clock test. |
| CLASSB_CLOCK_RTC_CLK_FREQ | RTC clock frequency. |
| CLASSB_CLOCK_TEST_RATIO_NS_MS | Ratio of mili second to nano second. |
| CLASSB_CLOCK_TEST_RTC_RATIO_NS | Duration of RTC clock in nano seconds. |
| CLASSB_COMPL_RESULT_ADDR | Address of one's complement test results. |
| CLASSB_INTERRUPT_COUNT_VAR_ADDR | Address of the variable which keeps interrupt count. |
| CLASSB_INTERRUPT_TEST_VAR_ADDR | Address of the variable which keeps interrupt test internal status. |
| CLASSB_INTR_DEVICE_VECT_OFFSET | Defines the offset for first device specific interrupt. |
| CLASSB_INTR_MAX_INT_COUNT | Defines the upper limit for interrupt count. |
| CLASSB_INTR_TEST_RTC_COUNT | Defines the counter value for RTC peripheral. |
| CLASSB_INTR_TEST_TC_COUNT | Defines the counter value for TC0 peripheral. |
| CLASSB_INTR_VECTOR_TABLE_SIZE | Defines the size of the vector table. |
| CLASSB_INVALID_TEST_ID | Invalid test ID. |
| CLASSB_ONGOING_TEST_VAR_ADDR | Address at which the ID of ongoing test is stored. |
| CLASSB_RESULT_ADDR | Address of test results. |
| CLASSB_SRAM_APP_AREA_START | Defines the start address of the SRAM for the application. |
| CLASSB_TEST_IN_PROG_VAR_ADDR | Address of the variable which indicates that a Class B test is in progress. |
| CLASSB_WDT_TEST_IN_PROG_VAR_ADDR | Address of the variable which indicates that a WDT test is in progress. |
| Name | Description |
|---|---|
| CLASSB_CPU_PC_TEST_VALUES | Data type for PC Test input and output values. |
| CLASSB_INIT_STATUS | Identifies Class B initialization status. |
| CLASSB_PORT_INDEX | PORT index definitions for Class B library I/O pin test. |
| CLASSB_PORT_PIN | PIN definitions for Class B library I/O pin test. |
| CLASSB_PORT_PIN_STATE | PORT pin state. |
| CLASSB_RST_RESULT_BF | Pointer to the structure for the Class B library run-time self-test result. This can be used to point to the result address 0x20000004. It will help to see the result in text form via watch window. |
| CLASSB_SST_RESULT_BF | Pointer to the structure for the Class B library startup self-test result. This can be used to point to the result address 0x20000000. It will help to see the result in text form via watch window. |
| CLASSB_STARTUP_STATUS | Identifies startup test status. |
| CLASSB_TEST_ID | Identifies Class B library tests. |
| CLASSB_TEST_STATE | Identifies Class B library test state. |
| CLASSB_TEST_STATUS | Identifies result from Class B library test. |
| CLASSB_TEST_TYPE | Identifies type of the Class B library test. |
| Name | Description |
|---|---|
| CLASSB_App_WDT_Recovery | This function is called if a WDT reset has happened during run-time. |
| CLASSB_CPU_RegistersTest | This self-test checks the processor core registers. |
| CLASSB_CPU_PCTest | This self-test checks the Program Counter register (PC). |
| CLASSB_ClearTestResults | Clears the results of SSTs or RSTs. |
| CLASSB_ClockTest | This self-test checks whether the CPU clock frequency is within the permissible limit. |
| CLASSB_FLASH_Callback | This function is used for interrupt callback. |
| CLASSB_FLASH_ECC_InterruptHandler | This function is called if FLASH ECC interrupt occurs. |
| CLASSB_FLASH_EccInit | Initialize ECC to perform fault detection on FLASH. |
| CLASSB_GetTestResult | Returns the result of the specified self-test. |
| CLASSB_GlobalsInit | This function initializes the global variables for the classb library. |
| CLASSB_IO_InputSamplingEnable | Enable input sampling for an IO pin. |
| CLASSB_Init | This function is executed on every device reset. This shall be called right after the reset, before any other initialization is performed. |
| CLASSB_SelfTest_FailSafe | This function is called if any of the non-critical tests detects a failure. |
| CLASSB_SRAM_Callback | This function is used for interrupt callback. |
| CLASSB_SRAM_ECC_InterruptHandler | This function is called if SRAM ECC interrupt occurs. |
| CLASSB_SRAM_EccInit | Initialize ECC to perform fault detection on SRAM. |
| CLASSB_SST_InterruptTest | This self-test checks basic functionality of the interrupt handling mechanism. |
| CLASSB_SST_WDT_Recovery | This function is called if a WDT reset has happened during the execution of an SST. |
| CLASSB_Startup_Tests | This function executes all startup self-tests inserted into classb.c file. |
| CLASSB_RST_IOTest | This self-test can be used to perform plausibility checks on IO pins. |
| CLASSB_TestWDT | This function tests the WatchDog Timer (WDT). |