1.7 USART Driver Asynchronous - UART Echo

This example echoes the received characters over the console using the USART driver in asynchronous mode.

Description

This example uses the USART driver in asynchronous mode in Bare-Metal environment to communicate over the console. It receives and echo’s back the characters entered by the user.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/usart/async/usart_echo/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
cec1736_evb.XMPLABX project for CEC 1736 Development Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
cec1736_evb.XCEC 1736 Development Board

Setting Up CEC 1736 Development Board

  • Connect the USB port P2 on the board to the computer using a micro USB cable

Running the Application

  1. Open the Terminal application (Ex.:Tera term) on the computer
  2. Connect to the Virtual COM port and configure the serial settings as follows:
    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  3. Build and Program the application using its IDE
  4. The console displays the following message
  5. Type a line of characters and press the Enter key
    Note: Number of characters entered before pressing enter key must be less than 256.
  6. Entered line will be echoed back and the LED is toggled
Refer to the following table for LED name: