1 Introduction
-
Two commonly used CRC standards are supported:
-
16-bit CRC-CCITT
-
32-bit CRC
-
-
Two software implementations are supported:
-
Look-up Table (LUT): This uses a CRC look-up table to speed up the computations. The look-up table requires 512 (for 16-bit) or 1024 (for 32-bit) bytes of Flash memory.
-
Direct computation: This calculates the checksum for each byte using a polynomial division. This version occupies less space in the Flash memory but is slower than the look-up table method.
-
Note: The AoUs listed in the Assumption of Use section below shall be followed to ensure correct operation. The Examples section shows how to follow some of the AoUs for different use cases and different devices.
-
AoU-FLASH_MEMORY_CHECKSUM_CRC_TEST-01: Case 1 shown in Table 1 shall not be used when the Flash CRC test is included in the application.
Reason: Since Case 1 configures the entire Flash as a BOOT section, the NVM controller will not be able to write to any address in the Flash and to store the calculated CRC value as a result. -
AoU-FLASH_MEMORY_CHECKSUM_CRC_TEST-02: The end address of the flash must be restricted through linker options in the following way, given each case presented in Table 1:
Case 1: shall not be used Case 2: the Flash shall be restricted to end at BOOTEND Case 3: the Flash shall be restricted to end at BOOTEND Case 4: the Flash shall be restricted to end at APPEND by adding the linker option: -Wl,--defsym=__TEXT_REGION_LENGTH__=new_length where: Case 1: Not used Case 2: new_length = size of the BOOT section Case 3: new_length = size of the BOOT section Case 4: new_length = size of the BOOT section + size of the APPCODE section Reason: This ensures that the linker does not place the Flash write routines, provided in the NVMCTRL driver, in the same section that it is writing to. Additionally, it ensures that storing the CRC bytes does not overwrite any program code or program data in the Flash. Please refer to the device data sheet under the NVMCTRL section for more information. Note that in MPLAB® X, such a linker option can be added by going to Project Properties> XC8 Global Options> XC8 Linker and adding the command in "Additional Options". -
AoU-FLASH_MEMORY_CHECKSUM_CRC_TEST-03: It is the responsibility of the system integrator to ensure that the store address for the CRC bytes resides in the following section, given each case presented in Table 1:
Case 1: Shall not be used Case 2: APPCODE Case 3: APPDATA Case 4: APPDATA Reason: Routines running in the BOOT Flash section can only write to the APPCODE and APPDATA Flash sections. Routines running in the APPCODE Flash section can only write in the APPDATA Flash sections. Routines running in the APPDATA Flash sections cannot write to any Flash section. -
AoU-FLASH_MEMORY_CHECKSUM_CRC_TEST-04: It is the responsibility of the system integrator to ensure that the memory section where the CRC bytes are stored, defined by the value of the store address, does not overlap with any other data used by the application.
Table 1: Flash Section Locations given Fuse settings (adapted from AVR128DA48 device data sheet).
|
Case |
BOOTSIZE* |
CODESIZE** |
BOOT Section |
APPCODE Section |
APPDATA Section |
|---|---|---|---|---|---|
|
1 |
0 |
- |
0 to FLASHEND |
- |
- |
|
2 |
> 0 |
0 |
0 to BOOTEND |
BOOTEND to FLASHEND |
- |
|
3 |
> 0 |
≤ BOOTSIZE* |
0 to BOOTEND |
- |
BOOTEND to FLASHEND |
|
4 |
> 0 |
> BOOTSIZE* |
0 to BOOTEND |
BOOTEND to APPEND |
APPEND to FLASHEND |
*Fuse names may differ between device families (BOOTSIZE on AVR DA devices and BOOTEND on Tiny1 devices), but the functionality is the same.
**Fuse names may differ between device families (CODESIZE on AVR DA devices and APPEND on Tiny1 devices), but the functionality is the same.-
Case 2: Using the fuse values equal to BOOTSIZE = 0x7F and CODESIZE = 0x0 results in a BOOT section with a size of 0x7F * 0x200 = 0xFE00, an APPCODE section with size of one block (0x200 bytes) and no APPDATA section. In this configuration, the storeAddress of the CRC bytes must reside in the APPCODE section and the following linker flag must be used:
-Wl,--defsym=__TEXT_REGION_LENGTH__=0xFE00 where all the program code and data will be placed inside the BOOT section by the linker. -
Case 3: Using the fuse values equal to BOOTSIZE = 0x7F and CODESIZE = 0x1 results in a BOOT section with a size of 0x7F * 0x200 = 0xFE00 bytes, no APPCODE section and an APPDATA section equal to one block (0x200 bytes). In this configuration, the storeAddress of the CRC bytes must reside in the APPDATA section and the following linker flag must be used: -Wl,--defsym=__TEXT_REGION_LENGTH__=0xFE00
where all the program code and data will be placed inside the BOOT section by the linker. -
Case 4: Using the fuse values equal to BOOTSIZE = 0x1 and CODESIZE = 0x7F results in a BOOT section with a size equal to one block (0x200 bytes), an APPCODE section with a size of (0x7F – 0x1) * 0x200= 0xFC00 bytes and an APPDATA section equal to one block (0x200 bytes). In this configuration, the storeAddress of the CRC bytes must reside in the APPDATA section and the following linker flag must be used (where the size of the BOOT section + size of the APPCODE section = 0x200 + 0xFC00 = 0xFE00):
-Wl,--defsym=__TEXT_REGION_LENGTH__=0xFE00 where all the program code and data will be placed inside both the BOOT and APPCODE section by the linker (unless otherwise specified by other linker options to place a bootloader in the BOOT section for instance). -
Note: It is possible to reserve more than one block in APPCODE (case 2) or APPDATA (case 3 and 4) if required. Taking case 2 as an an example: Using the fuse values equal to BOOTSIZE = 0x50 and CODESIZE = 0x0 results in a BOOT section with a size of 0x50 * 0x200 = 0xA000, an APPCODE section with the size of 0x30 blocks (0x6000 bytes) and no APPDATA section. In this configuration, the storeAddress of the CRC bytes must reside in the APPCODE section and the following linker flag must be used: -Wl,--defsym=__TEXT_REGION_LENGTH__=0xA000 where all the program code and data will be placed inside the BOOT section by the linker.
-
Case 2: Using the fuse values equal to BOOTEND = 0x3F and APPEND = 0x0 results in a BOOT section with a size of 0x3F * 0x100 = 0x3F00, an APPCODE section with size of one block (0x100 bytes) and no APPDATA section. In this configuration, the storeAddress of the CRC bytes must reside in the APPCODE section and the following linker flag must be used:
-Wl,--defsym=__TEXT_REGION_LENGTH__=0x3F00 where all the program code and data will be placed inside the BOOT section by the linker. -
Case 3: Using the fuse values equal to BOOTEND = 0x3F and APPEND = 0x1 results in a BOOT section with a size of 0x3F * 0x100 = 0x3F00 bytes, no APPCODE section and an APPDATA section equal to one block (0x100 bytes). In this configuration, the storeAddress of the CRC bytes must reside in the APPDATA section and the following linker flag must be used:
-Wl,--defsym=__TEXT_REGION_LENGTH__=0x3F00 where all the program code and data will be placed inside the BOOT section by the linker. -
Case 4: Using the fuse values equal to BOOTEND = 0x1 and APPEND = 0x3F results in a BOOT section with a size equal to one block (0x100 bytes), an APPCODE section with a size of (0x3F – 0x1) * 0x100= 0x3E00 bytes and an APPDATA section equal to one block (0x100 bytes). In this configuration, the storeAddress of the CRC bytes must reside in the APPDATA section and the following linker flag must be used (where the size of the BOOT section + size of the APPCODE section = 0x100 + 0x3E00 = 0x3F00):
-Wl,--defsym=__TEXT_REGION_LENGTH__=0x3F00 where all the program code and data will be placed inside both the BOOT and APPCODE section by the linker (unless otherwise specified by other linker options to place a bootloader in the BOOT section for instance). -
Note: It is possible to reserve more than one block in APPCODE (case 2), APPDATA (cases 3 and 4) and BOOT (case 4) if required. Taking case 4 as an example: Using the fuse values equal to BOOTEND = 0x5 and APPEND = 0x20 results in a BOOT section with a size equal to 0x5 blocks (0x500 bytes), an APPCODE section with a size of (0x20 – 0x5) * 0x100 = 0x1500 bytes and an APPDATA section equal to 0x40 - 0x20 - 0x5 = 0x1B blocks (0x1B00 bytes). In this configuration, the storeAddress of the CRC bytes must reside in the APPDATA section and the following linker flag must be used (where the size of the BOOT section + size of the APPCODE section = 0x500 + 0x1500 = 0x1A00):
-Wl,--defsym=__TEXT_REGION_LENGTH__=0x1A00 where all the program code and data will be placed inside both the BOOT and APPCODE section by the linker (unless otherwise specified by other linker options to place a bootloader in the BOOT section for instance).