24.4.13 Assigning Objects to Sections
The __section() specifier can be used to indicate that an
object should be located in the named section. This is typically used when the object has
special and unique linking requirements that cannot be addressed by existing compiler
features.
Use the native keywords discussed in the Differences section to look up information on the semantics of this specifier.
Example
The following shows a variable which uses the __section
keyword.
int __section(“comSec”) commonFlag;
Differences
The 8-bit compilers have previously used the #pragma psect directive to
redirect objects to a new section, or psect; however, the __section()
specifier is the preferred method to perform this task, even if you are not using the
CCI.
The 16- and 32-bit compilers have used the section attribute to indicate a
different destination section name. The __section() specifier works in a
similar way to the attribute.
Migration to the CCI
For MPLAB XC8, change any occurrence of the #pragma psect directive, such
as:
#pragma psect text%%u=myText
int getMode(int target) {
//...
}
to the __section() specifier, as in:
int __section ("myText") getMode(int target) {
//...
}
For 16- and 32-bit compilers, change any occurrence of the section
attribute, for example, from:
int __attribute__((section(“myVars”))) intMask;
to:
int __section(“myVars”) intMask;
Caveats
None.