9.10.2 aligned
(alignment)
This attribute specifies a minimum alignment for the variable, measured in bytes. The alignment must be a power of two. For example, the declaration:
int x __attribute__ ((aligned (16))) = 0;
causes the compiler to allocate the global variable x
on a 32-bit MCU-byte boundary. On thePIC32A MCU device, this could be used in conjunction
with an asm expression to access DSP instructions and addressing modes
that require aligned operands.
As in the preceding example, you can explicitly specify the alignment (in bytes) that you wish the compiler to use for a given variable. Alternatively, you can leave out the alignment factor and just ask the compiler to align a variable to the maximum useful alignment for the PIC32A MCU device. For example, you could write:
short array[3] __attribute__ ((aligned));
Whenever you leave out the alignment factor in an aligned attribute specification, the compiler automatically sets the alignment for the declared variable to the largest alignment for any data type on the target machine – which in the case of the PIC32A MCU device is two bytes (one word).
The aligned attribute can only increase the alignment;
you can decrease it by specifying packed (see below). The
aligned attribute conflicts with the reverse
attribute. It is an error condition to specify both.
The aligned attribute can be combined with the
section attribute. This will allow the alignment to take place in a
named section. By default, when no section is specified, the compiler will generate a
unique section for the variable. This will provide the linker with the best opportunity
for satisfying the alignment restriction without using internal padding that may happen
if other definitions appear within the same aligned section.