28.2.69 __builtin_sftac
Description
Shifts accumulator by shift. The valid shift range is
-32 to 32.
For example:
volatile register int32_t result asm(“A”);
int32_t i;
result = __builtin_sftac(result,i);
Might generate:
sftac A, w0
Prototype
int32_t __builtin_sftac(int32_t Accum, int32_t shift);
Arguments
Accum – Accumulator to shift.
shift – Amount to shift.
Return Value
Returns the shifted result to an accumulator.
Machine Instruction
sftac
Error Messages
An error message will be displayed if:
- the result is not an accumulator register
Accumis not an accumulator register- the shift value is not a literal within range