22.5 Integers

Implementation-Defined Behavior for Integers is covered in section G.3.5 of the ANSI C Standard.

The following table describes the amount of storage and range of various types of integers: (ISO 6.1.2.5)

Table 22-2. Integer Types
DesignationSize (bits)Range
char8-128 ... 127
signed char8-128 ... 127
unsigned char80 ... 255
short16-32768 ... 32767
signed short16-32768 ... 32767
unsigned short160 ... 65535
int32-2147483648 ... 2147483647
signed int32-2147483648 ... 2147483647
unsigned int320 ... 4294867295
long32-2147483648 ... 2147483647
signed long 32-2147483648 ... 2147483647
unsigned long320 ... 4294867295
long long64-9223372036854775808 ... 9223372036854775807
signed long long64-9223372036854775808 ... 9223372036854775807
unsigned long long640 ... 18446744073709551615

What is the result of converting an integer to a shorter signed integer, or the result of converting an unsigned integer to a signed integer of equal length, if the value cannot be represented? (ISO 6.2.1.2)

There is a loss of significance. No error is signaled.

What are the results of bitwise operations on signed integers? (ISO 6.3)

Shift operators retain the sign. Other operators act as if the operand(s) are unsigned integers.

What is the result of a right shift of a negative-valued signed integral type? (ISO 6.3.7)

The sign is retained.