1.2.2.1 Known Issues
Note: This section is maintained from Release
v3.14.0. Refer to release notes for other releases known
issue.
Issue Details | Affected Version | Workaround/Remarks | Is fixed? | Issue fixed Version |
---|---|---|---|---|
Touch configurator not loading for PIC32WM_BZ6204 | 3.18.0 | Needs to be fixed. | Yes | 3.18.1 |
The Touch Library is not compatible with the new variants of the PIC32CMJH device family: PIC32CM(3204|6408)JH000(32|48|64). These variants are newly added in the recent released part-pack (DFP) version 1.3.221 | 3.17.0 | We would address this in the next release of H3 Touch package v3.18.0 | Yes | 3.18.0 |
sync busy code missing for TC/TCC in timer-based Driven Shield projects. | 3.17.0 | Needs to be fixed. | Yes | 3.18.0 |
touch library path issues for TrustZone® devices. | 3.17.0 | Needs to be fixed. | Yes | 3.18.0 |
Projects created for the PIC32WM_BZ6 device are currently experiencing compilation issues with the existing compiler (v4.45). | 3.17.0 | Please await the next compiler release (v4.60), which will include a resolution for this problem. | Yes | 3.18.0 |
For Trust-zone devices, RTC configured by Touch didn't work. | 3.15.0 | Call touch_init after RTC_Initialize in the SYS_Initialize function. | No | Not applicable. |
Touch Configurator doesn't retain the pins selected for Mutual capacitance matrix view while reopening. | 3.16.0 | Needs to be fixed. | No | Not applicable. |
For Trust-zone devices, some Touch lines didn't work due to default configuration bits generated in initialization function. | 3.16.0 | Manually edit the configuration bits. | No | Not applicable. |
Timer based driven shield project may not work for SAM C2x, SAM L22 | 3.15.0 | Needs to be fixed. | Yes | 3.16.0. |
For Trust-zone devices,there is code compilation when boost mode feature is selected. | 3.14.0, 3.15.0,3.16.0 | Needs to be fixed. | No | Not applicable. |
Unable to select timer pins in timer based driven shield projects. | 3.14.0 | Needs to be fixed. | Yes | 3.15.0 |
Code generation fails when Boost mode + Surface options are used | 3.14.0 | Needs to be fixed. | Yes | 3.15.0 |
Unable to select 1T surface project without gesture option | 3.14.0 | Needs to be fixed. | Yes | 3.15.0 |
Software Low power is not working on PIC32CZ CA | 3.14.0 | Needs to be fixed. | Yes | 3.15.0 |
PIC32MZDA code compilation error | 3.14.0 | Needs to be fixed. | Yes | 3.15.0 |
Enable Driven shield Plus option is visible for 1 button. Whereas Driven shield Plus options is valid for more than one button. | 3.14.0 | Do not enable Driven Shield Plus option with one button | No | Not applicable |
Entering more than 9 in surface segments is not working. | 3.14.0 | Needs to be fixed. Use up and down arrows to increase the surface segment | No | Not applicable |
Reset Pin assignment option is removed. | 3.14.0 | Yet to be implemented. Reassign pins for each sensor. | No | Not applicable |
Sync all option for sensor parameter is not available. | 3.14.0 | Yet to be implemented. Assign values for each sensor. | Yes | 3.15.0 |
Unable to dock Touch Configurator window within MPLAB®X IDE. | 3.14.0 | Needs to be fixed. No issue with respect to functionality. Waiting on external dependency. | No | Not applicable |