3.3.1.1 DEF_TOUCH_MEASUREMENT_PERIOD_MS
This parameter defines the measurement period in milliseconds. The timer interrupt service routine (ISR) will be set up according to this value. If the specified time is shorter than the measurement period, the touch measurement will occur consecutively without any breaks.
Range | 1 to 255 |
---|---|
Default Value | 20 |
The following figure shows the measurement period and measurement time.