1.1.2 Generate Touch Project with MCC Melody
Objective
The following procedure shows how to create a Touch project with the MCC Melody platform where touch sensors and their parameters can be graphically added and tuned. The resulting project supports the MPLAB® XC8 compiler in MPLAB®X IDE. This project uses the ATTINY3217 Xplained Pro board along with the T10 Mutual Capacitance Xplained Pro Extension Kit.
Materials
Hardware Tools
Software Tools
MPLAB®X IDE with MCC installed.
Procedure
Step 1: Open MPLAB®X IDE
Click and select the File > New Project option in MPLAB® X IDE.
Step 2: Choose Project
In the New Project window, select Application Project and click Next.
Type TINY3217 in the Device option and select ATtiny3217.
In the Tool option, select the Attiny3217 Xplained Pro Tool form the drop down and click Next.
Step 4: Compiler Selection
In the Select Compiler section, select the XC8 compiler and click Next.
Step 5: Project Settings
Enter the project name, location and folder for the project and click Finish.
Step 6: MCC with Melody
Select MCC from the Toolbar
The MCC content Manager window opens and from it click Next in MCC Melody.
Step 7: Melody with Touch package
Select the Touch content from the Optional Content section and click Finish.
Add Touch from Touch configurator from th Device Resources Tab.
Touch is added to the Project graph as shown below.
Include RTC from Device Resources
The builder with RTC and Touch is as follows.
Enable Overflow Interrupt in RTC.
Select Mutual cap from the drop down as shown.
Click Button icon and add 4 buttons
The following dialog box opens indicating that the Sensor pins are auto assigned on creation. Click Ok.
Now click Slider and select 4 in segments and click Add.
Now 4 buttons and 4 channel slider sensor are added.
A generalized pin assignment for a majority of the Xplained PROs and MCUs have been provided in a downloadable file titled "Curiosity Nano Touch Adapter Pin Configurattion" the Documentation section in this link as shown in the figure.
If the MCU or the XPRO board is not available then the user can assign the pins based on the datatsheet/userguide of that particular MCU/ XPRO. A snapshot of the pinout for SAML10 and T10 XPRO can be seen from the below figure.
Based on the documentation file, the X and Y lines should be selected as follows.
Sensor | Channel ID | X Line | Y Line |
Button 0 | 0 | 5 | 4 |
Button 1 | 1 | 4 | 4 |
Button 2 | 2 | 1 | 4 |
Button 3 | 3 | 0 | 4 |
Slider 0 | 4 | 5 | 3 |
5 | 4 | 3 | |
6 | 1 | 3 | |
7 | 0 | 3 |
The pin assignement can be done in Configure → Sensor Pins. With respect to the above table in touch configurator the pins were selected.
Parameters
Step 13: Sensor Parameters
For tuning the touch parameters, Config → Sensor Parameters and tune according to the application.
The Sensor Parameters Tab allows to configure touch sensor parameters such as:
- Digital Filter Gain
- Digital Filter Oversampling
- Analog Gain
- Series Resistor
- Addition Charge Share Delay
- PTC Clock
- Sensor Detect Threshold
- Sensor Hysteresis
- Sensor AKS
Here the CPU operating frequency can be set in the GCLK block in MHz as highlighted above.
Step 14: Common Parameters
For tuning the touch parameters, Config → Common Parameters and tune according to the application.
The Common Parameters Tab allows to configure touch sensor parameters such as:
- Acquisition
- Scan Rate
- PTC Interrupt Priority
- Acquisition Frequency
- Sensor
- Detect Integration
- Away from Touch Recal Integration count
- Away from Touch Recal Threshold
- Touch Drift Rate
- Away from touch Drit Rate
- Drift Hold Time
- Re-burst mode
- Max ON Duration
Step 15: Frequency Hop:
Frequency Hop can be enabled by navigating to Config → Frequency Hop and then sliding the Enable Frequency Hop button. A maximum of 7 frequency steps can be selected which can be induvidually configured using the drop down. Hop Frequencies are fixed at compile time in Frequency Hop.
The auto-tune feature can be enabled by sliding the Enable Frequency Auto Tuning button. A detailed description on how to configure the Frequency Hop and Frequency Hop Autotune is provided in the How to Enable Frequency Hop Auto tune page.
Step 16: Touch Tuning
Enable the datastreamer by selecting the Enable Touch tuning Data connection option. A detailed description on how to configure the datastreamer is provided in the Guide to view Touch Tune Data using MPLAB® Data Visualizer page.
Click on the Summary Tab to review the project configuration and find versions of Library modules. Check whether all the necessary paramneters are enabled and present.
The pins assignment can be checked as configured above in the Pin Grid View.
Step 18: Configuring Hints and Warnings
In Notifications Tab, it can be seen that a few hints and warning have been given for the project to build without any errors.
To clear these hints and warning, in Touch Configurator → Click Important Notes.
A new pop up with the notifications and a checkbox is displayed. Once all the items in the notificaitons are checked, the warnings and hints are cleared.
In the Resource management tab select Interrupt Manager and enable the Global interrupt as indicated in the Hints.
Now click Generate from the Project Resources Tab.
The Generation complete message is displayed in the output window.
Step 19: Include touch_process() to the main while(1) loop. Now the project is ready for testing on the kit.