1.2.2.1 Known Issues
Note: This section is maintained from Release
v3.14.0. Refer to release notes for other release known issues.
| Issue Details | Affected Version | Work Around/Remarks | Is Fixed? | Issue Fixed Version |
|---|---|---|---|---|
|
The Touch library is not compatible with the new variants of the PIC32CMJH device family: PIC32CM(3204|6408)JH000(32|48|64). These variants are newly added in the recent released part-pack (DFP) version 1.3.221. | 3.17.0 | To be addressed in the next release of H3 Touch package v3.18.0 | No | Not applicable |
| Projects created for the PIC32WM_BZ6 device are currently experiencing compilation issues with the existing compiler (v4.45) | 3.17.0 | The next compiler release (v4.60) will include a resolution for this problem | No | Not applicable |
| For Trust-zone devices, RTC configured by Touch didn’t work | 3.15.0 | Call touch_init after
RTC_Initialize in the
SYS_Initialize function. | No | Not applicable |
| Touch Configurator doesn’t retain the pins selected for the Mutual capacitance matrix view while reopening | 3.16.0 | Needs to be fixed | No | Not applicable |
| For Trust-zone devices, some Touch lines didn’t work due to default configuration bits generated in the initialization function | 3.16.0 | Manually edit the configuration bits | No | Not applicable |
| Timer-based Driven Shield project may not work for SAM C2x, SAM L22 | 3.15.0 | Needs to be fixed | Yes | 3.16.0 |
| For Trust-zone devices,there is code compilation when Boost mode feature is selected |
3.14.0 3.15.0 3.16.0 | Needs to be fixed | No | Not applicable |
| Unable to select timer pins in timer-based Driven Shield projects | 3.14.0 | Needs to be fixed | Yes | 3.15.0 |
| Code generation fails when Boost mode + Surface options are used | 3.14.0 | Needs to be fixed | Yes | 3.15.0 |
| Unable to select 1T surface project without gesture option | 3.14.0 | Needs to be fixed | Yes | 3.15.0 |
| Software Low power is not working on PIC32CZ CA | 3.14.0 | Needs to be fixed | Yes | 3.15.0 |
| PIC32MZDA code compilation error | 3.14.0 | Needs to be fixed | Yes | 3.15.0 |
| The Enable the Driven Shield Plus option is visible for one button. Whereas Driven Shield Plus options are valid for more than one button. | 3.14.0 | Do not enable Driven Shield Plus option with one button | No | Not applicable |
| Entering more than 9 in surface segments is not working | 3.14.0 |
Needs to be fixed. Use up and down arrows to increase the surface segment. | No | Not applicable |
| The Reset Pin assignment option is removed | 3.14.0 |
Yet to be implemented. Reassign pins for each sensor. | No | Not applicable |
| Sync all option for sensor parameter is not available | 3.14.0 |
Yet to be implemented. Assign values for each sensor. | Yes | 3.15.0 |
| Unable to dock Touch Configurator window within MPLAB® X IDE | 3.14.0 |
Needs to be fixed. No issue with respect to functionality. Waiting on external dependency. | No | Not applicable |