1.2.2.1 Known Issues

Note: This section is maintained from Release v3.14.0. Refer to release notes for other release known issues.
Issue DetailsAffected VersionWork Around/RemarksIs Fixed?Issue Fixed Version
Selecting driven shield feature option for SAMC2x and PIC32CM(3204|6408)JH000(32|48|64) doesn't work as expected3.20.0Open MCC and select System icon, Modify the DMA Beat size of Channel 0 from 16-bit bus transfer to 32-bit bust transfer.NoNot applicable

The Touch library is not compatible with the new variants of the PIC32CMJH device family: PIC32CM(3204|6408)JH000(32|48|64).

These variants are newly added in the recent released part-pack (DFP) version 1.3.221.

3.17.0To be addressed in the next release of H3 Touch package v3.18.0YesNot applicable
Projects created for the PIC32WM_BZ6 device are currently experiencing compilation issues with the existing compiler (v4.45)3.17.0The next compiler release (v4.60) will include a resolution for this problemYesNot applicable
For Trust-zone devices, RTC configured by Touch didn’t work3.15.0Call touch_init after RTC_Initialize in the SYS_Initialize function.NoNot applicable
Touch Configurator doesn’t retain the pins selected for the Mutual capacitance matrix view while reopening3.16.0Needs to be fixedNoNot applicable
For Trust-zone devices, some Touch lines didn’t work due to default configuration bits generated in the initialization function3.16.0Manually edit the configuration bitsNoNot applicable
Timer-based Driven Shield project may not work for SAM C2x, SAM L223.15.0Needs to be fixedYes3.16.0
For Trust-zone devices,there is code compilation error when Boost mode feature is selected

3.14.0

3.15.0

3.16.0

Needs to be fixedYesNot applicable
Unable to select timer pins in timer-based Driven Shield projects3.14.0Needs to be fixedYes3.15.0
Code generation fails when Boost mode + Surface options are used3.14.0Needs to be fixedYes3.15.0
Unable to select 1T surface project without gesture option3.14.0Needs to be fixedYes3.15.0
Software Low power is not working on PIC32CZ CA3.14.0Needs to be fixedYes3.15.0
PIC32MZDA code compilation error3.14.0Needs to be fixedYes3.15.0
The Enable the Driven Shield Plus option is visible for one button. Whereas Driven Shield Plus options are valid for more than one button.3.14.0Do not enable Driven Shield Plus option with one buttonNoNot applicable
Entering more than 9 in surface segments is not working3.14.0

Needs to be fixed.

Use up and down arrows to increase the surface segment.

NoNot applicable
The Reset Pin assignment option is removed3.14.0

Yet to be implemented.

Reassign pins for each sensor.

NoNot applicable
Sync all option for sensor parameter is not available3.14.0

Yet to be implemented.

Assign values for each sensor.

Yes3.15.0
Unable to dock Touch Configurator window within MPLAB® X IDE3.14.0

Needs to be fixed.

No issue with respect to functionality. Waiting on external dependency.

NoNot applicable