5.2 Guide to View Touch Tune Data Using MPLAB® Data Visualizer

This section provides information on how to visualize touch data when a bidirectional connection is enabled in the Touch Configurator.

Project Configuration and Generation

For creating and configuring a project for visualization, follow the steps in the Generate a Touch Project With MCC Melody section in the case of MPLAB® Code Configurator (MCC) Melody, or the Generate Touch Project With MCC Harmony section in the case of MCC Harmony.

After the creation and configuration of the sensors, navigate to the Tune tab in the Touch Configurator, toggle the Enagle Touch Tuning Data connection button and select Touch Tuning as the option.

Data Visualization

Open the MPLAB® Data Visualizer plug in/stand alone and follow the steps given below for Touch visualization and tuning.

Refer Step-by-Step Procedure for Touch Plug-In Installation for Touch Plugin installation

The three main sections for data visualization are,

  • Connection
  • Configuration
  • Graph

Section I: Connection

Step 1: Baud Rate setup

Once the window is open, go to the Connections tab, select the correct COM port. In the COM port settings section, click the ‘Gear’ icon and set the Baud Rate required for the project.

Step 2: Touch COM port selection

In the Touch section, select the correct COM port form the drop down as the data source.

Step 3:

Now start the streaming on the COM port first and then start the streaming on the Touch section.

Section II: Configuration

Step 4: Selection of parameters

Select any one of the listed options other than Output Data. In this case, Sensor Node Parameters is selected.

Step 5: Modification of Parameters

Under the Sensor Node Config tab, select and modify any one of the parameters in the table.

Step 5: Writing to the kit

Once the required parameters are changed, the Write to kit button changes its color to yellow and it can be clicked. If the write is successful, the button will change to green, indicating success; otherwise, it will change to red, indicating an error with the kit.

Step 6: Reading from the kit

Click Read From Kit button to retrieve the configuration from the kit.

Section III: Graph

For CVD devices:

The Graph is automatically populated for Deviation and Pressed parameters for the sensors.

For PTC devices:

The Graph is automatically populated for State and Delta parameters for the sensors.

Surface Data Visualization:

i. Graph:

The graph displays touch points in a continuous, drawing-like manner, providing a clear and intuitive visualization of the touch path on the surface board.

ii. Gesture:

Access the Gesture tab to view information on the types of gestures executed on the surface board.