1.1.8 How to create Lump Sensor
Overview
This section provides step by step information for Generating Lump sensor using Touch Configurator in MCC.
Creating Lump
Step 1: Open Touch Configurator
Select MCC and open Touch Configurator in Resource Management (MCC) tab
Step 2: Create Buttons, Slider and Wheel.
Add the required number of Buttons, Sliders and Wheels
Step 3: Create Lump Button
Press control key and Click sensors ( Buttons/Sliders/Wheels) to be configured as Lump sensor.(Lump can also be created by mouse movement).Now click create Create Lump Sensor .
Step 4: Visualize Lump Sensor
Hexagon Graphic represents Lump sensors. The lumped individual sensors will be displayed in yellow when mouse cursor is placed over the lump sensor .
Step 5: Generate Lump Sensor Code
Click Generate in Resource Management (MCC) tab.
The following animation shows the process of creating a Lump sensor in Touch Configurator.