6.6 Nonce
Command
The Nonce command has the dual purpose of being used to output a random number for use by the system and/or to generate a session key for use by a subsequent
Write
command by the host. A single invocation of the Nonce command will result in the following:- A random number will be generated and output on the bus for use by the host system.
- An internal nonce value will be generated for use internally by the ECC204-TFLXAUTH.
- A session key will be generated if the proper input parameter is provided.