1.2 Secure MCC MDFU Client Library – Provisioning the Secure Element

This document explains the process of provisioning the secure element with the public key. The secure element for this example is the ATECC608B chip which is provisioned using Microchip’s Trust Platform Development Suite (TPDS).

Important: This document explains the prototyping use case for provisioning. For production, follow the production steps. The support document is linked here.

The hardware secure element used for the development and testing of the 8-bit Secure MDFU Client is the ATECC608 Trust development board, but any other click or development board with an ATECC608 chip can also be used for provisioning.

This example expects that the user has the secure hardware element and TPDS downloaded.

  1. Open TPDS by clicking the Start icon on your PC and searching for “Trust Platform Development Suite”.
    Figure 1-1. Open Trust Platform Development Suite
  2. A command prompt will pop up and load the TPDS application. The homepage will appear on the screen once loaded. Click the Configurators tab on the top gray bar.
    Figure 1-2. Configurators Tab
  3. Click the ATECC608-TFLXTLS Configurator under ATECC608-TFLXTLS.
    Figure 1-3. Open the ATECC608-TFLXTLS Configurator
  4. The screen displays different available use cases for the selected secure element. Clicking each use case highlights the recommended key slots that can be used.
  5. In this example, key slot 13 is used to store a parent public key. Click Slot 13 under the Slot Number column.
    Figure 1-4. Slot 13 Description
  6. Upload the public key either by entering the raw hex data or by directly uploading the .pem file.
    Figure 1-5. Upload Public Key in TPDS
  7. After uploading the .pem file or entering the hex data, click the Verify button.
    Figure 1-6. Verify Public Key Data
  8. After clicking the Verify button, a pop-up window will display the entered data, verify the data again and click the OK button.
    Figure 1-7. Verify Public Key Data in Pop-Up
  9. For prototyping, it is recommended to keep the “Disable Slot Write” check box unchecked.
    Figure 1-8. Keep Disable Write Slot Unchecked
  10. Scroll down until the Prototyping and Production steps are visible.
  11. Click the Generate Provisioning Package button.
    Figure 1-9. Click on Generate Provisioning Package
  12. Verify where the path is saved and click the OK button.
    Figure 1-10. Verify Path for Package Download
  13. Click the Provision Prototype Sample button.
    Figure 1-11. Provision Prototype Samples
  14. Upload the generated package from Downloads.
    Figure 1-12. Upload Generated Package
  15. The DIP switches (if any) on the secure element need to be switched on for the provisioning to be successful.
    Tip: The element may need to be disconnected and reconnected several times if failures are observed.
  16. A pop-up will display if the provisioning is successful.
    Figure 1-13. Provisioning Complete
  17. The secure element is now ready to be used for the ECDSA verification.