4.2.4.8 NWK_JoinControl_t Struct
C
typedef struct _NWK_JoinControl_t
{
/** The method of joining the network. */
NWK_JoinMethod_t method;
/** If this parameter is TRUE than NWK layer will encrypt all NWK packet
* during join procedure. It means that if the method parameter is equal
* to NWK_JOIN_VIA_REJOIN than NWK layer will encrypt rejoin request
* command and will expect encrypted rejoin response command. */
bool secured;
/** TRUE means that NWK performs active scan to discover networks in
* neighborhood otherwise NWK uses the neighbor table as is. In that
* case (FALSE value), you can put all known neighbors to the neighbor table
* before join and NWK will try to join only to these neighbors. */
bool discoverNetworks;
/** Notify other ZigBee devices that the device has joined or re-joined the network. */
bool annce;
/** The flag indicates that the neighbor table must be cleared or not. */
bool clearNeighborTable;
} NWK_JoinControl_t;
Description
The type defines network join method and joining settings.