2.2.2 Monotonic Counter

SHA104 supports one nonvolatile monotonic counter that can count to a value of 10,000.

The counters can be used in one of two methods :
  • Cryptographic Counters:

    In this mode, the value of the counter can be read or incremented. It is the responsibility of the host to determine how this counter is used.

  • Limited Key Use:

    The monotonic counter can be attached to the Symmetric Key stored in Slot 3 to restrict the number of times this key can be used.