The MCC Content Manager (CMT) allows users to select specific versions of the component modules
and libraries to be used for their MCC projects. Refer to the
MCC Content Manager
Reference for more information.
The MCC Melody Content Manager, supports content management and
versioning at a component level.
This means that component modules of a
project can be updated on its own, separate from the other modules. For example, if you
have a working project, except for a bug on the ADC driver. Now, rather than needing to
update all the other drivers in your system, like the UART and Timers, you will be able to
update just the ADC.
This component level content versioning
granularity will be especially useful in the latter stages of your project development, as
you near production. At this stage, when almost everything is working perfectly, one may
want to change one modules one needs to, due to either bugs or needed features.
Figure 5-1. Opening the MCC Content Manager
Reference, MCC User Guide
DS40001829G
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.