5.4.1 How ITM Trace Works
All SAM MCUs/MPUs that support ITM trace are Arm® Cortex®-M processor-based devices with Arm® CoreSight® architecture. Currently ITM is supported in Cortex M3, M4, M33, and SC300 cores.
The CoreSight Instrumentation Trace Macrocell (ITM) block is a software application driven trace source. Supporting user code generates SoftWare Instrumentation Trace (SWIT). In addition, the block provides a coarse-grained timestamp functionality. The main uses for this block are to:
- support
printfstyle debugging. - trace OS and application events.
- emit diagnostic system information.
MPLAB ICD 5 is capable of streaming UART-format ITM trace to the host computer. Trace is captured on the TRACE/SWO pin of the 10-pin header (JTAG TDO pin). Data is buffered internally on the MPLAB ICD 5 and is sent over the trace interface to the host computer.
The ITM contains the following sub-blocks:
- Timestamp
-
Generates timestamp packet.
- Sync control
-
ITM synchronizer.
- Arbiter
-
Arbitrates between synchronous, timestamp, and SWIT packet.
- FIFO
-
ATB First In First Out (FIFO).
- Emitter
-
ATB registered emitter.
Data is written to the stimulus registers using the APB interface. This data is then transmitted on the ATB interface as SWIT packets .